I have several 1-bit images which I want to project one after the other.
My aim is to achieve highest image streaming rate ( with latencies at the level of milliseconds).
What is the fastest way of streaming images to the DLPC350? What are the latencies I can achieve using HDMI port and if I load the images in the flash drive? Also, if I use panda board, will it improve the streaming speed and display the images at high speed?
Also, I want to perform this process without using the GUI.