Hello,
I have another question regarding my own implementation of communication with the Projector.
Is it possible to get access to the code of the LightCrafter GUI or at least the part of it, where the communication with the device is handled? I am able to implement this functionality myself or at least parts of it, but I would rather not have to because it would take a lot of time.
Maybe there is an interface already available with some functions that send commands directly without having to handle the different types of packets, payload sizes and so on?
Also I am not able to test the things I have already implemented because of some *.dll issue with Cypress (see https://e2e.ti.com/support/dlp__mems_micro-electro-mechanical_systems/f/1006/t/441756