I know that according to the white paper on the subject,
"The specification is 25 W/cm2 input power in the visible spectrum, where the pixel reflectivity is about 92%,so that about 8% of the energy is absorbed by the pixel surface (2) (see Figure 7). For ranges outside the visible spectrum, use the power specification in the data sheet and the absorption for the wavelength being used."
I am using a low power laser at 532 nm. I'm not sure what data sheet is being referred to or where in the data sheet the requisite information can be found. Could you please point me in the right direction. Thank you.
(Please note that this is after successful removal of the LightEngine from the LightCrafter.)