This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Mounting DLP LightCrafter 6500



Hi. Can you please suggest some general ideas about how to mount DMD and controller board (DLP LightCrafter 6500) in an experimental setup? Would I need to make customized frames for then?

Thanks.

  • Hello Yongjin,

    Yes, the LightCrafter 6500 can be mounted to a customized frame. In your mounting setup, be sure that the flex cable between the boards does not bend with a radius less than 25.4 mm, and only bends between the two gold bands on the flex (not in the short space between each gold band and the board).

    Best regards,
    Trevor