Hello, I utilize DLP LightCrafter 6500EVM and I have already added 212 1 bit-patterns to the Firmware of the EVM.
There is no problem to update the 212 patterns and display the patterns.
But when I update the Firmware to add 1bit, 399 number of patterns, then an error is occurred as shown above.
Of course, prior to updating the Firmware, I browse the raw firmware file which has no existing patterns or batch files.
I cannot understand the error because TI introduces this EVM is capable of holding up to 400 1bit patterns...
Why this error occurs and how can I solve this?
Thanks.
212