Hi,
I am an engineer and I think the DLP 4500 crafter is very suitable for my further development. I want to use the DMD to generate 1000HZ light square wave. But there are two things I can not get the point.
1. I saw the cross over time is 3-µs. Does it mean that I can generate 1000HZ square light wave without worrying about the switch rate?
2. what does the Max Pattern Rate mean? Is it related with the max modulation rate.