This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I2C communication between arduino and DLP LightCrafter Display 4710



Hi!

I am trying to control my DLP LightCrafter Display 4710 throught in I2C via the J_DEV pins.

The board I am using to send I2C commands is an Arduino UNO.

Here is my Arduino code:

#include <Wire.h>

void setup()
{

  Serial.begin(9600);

  Wire.begin();
  Wire.beginTransmission(0x36);
  Wire.write(0X14);
  Wire.write(0x02);
  Wire.endTransmission();

  Serial.print("Data send\n");
}

void loop()
{

}

Normally, when I run the code, an I2C command should be send to the DLP to flip the screen but it doesn't works.

I tried to connect 2 arduino to test the I2C and the command is received by the slave (arduino).

I tried to pull-up SDA and SCL with 10k Ohms but it doesn't works.

I have no idea of why it doesn't works so if anyone can help on it this will be great!

Many thanks in advance!