Other Parts Discussed in Thread: DLPC350
Is there a way to increase the trigger edge control beyond ~20usec? We do not require the camera trigger to be active through the entire exposure time. The trigger is needed only to initiate the exposure. On long exposures (>1 sec), we have have a problem with the trigger line going inactive for (possibly) too brief a time before the next exposure. The line goes inactive for ~2ms before going active again for another >1sec period. We are not certain, but this may be causing some trigger edges to be missed by our cameras. If we could control the trigger line (TRIGGER OUT1) to be much less than the exposure time that could be helpful.