This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Dynamic control of image sequence using external trigger

Hi,

For my application I want to display a 24 bit image stored in flash as a sequence of 1-bit patterns. I will be using an external device to trigger the start of the sequence. But what I want is that the sequence of the images in the flash to be controlled by the external device bidirectionally, in other words, when an external positive trigger is generated by this external device,  the projector starts displaying pattern at G0 and with the next positive trigger, it should display the pattern at G1. But if the external device generates a negative trigger, than the sequence should starts moving backwards and display again the pattern at G0.

So my first question is that is this dynamic control is possible using flash as a source? I want to achieve high pattern rates and would prefer using flash as my source.

And my second questions, if not flash, then what is the other way to achieve this dynamic pattern sequencing?


Thanks in advance

Aamir