Does DLP4710 support side illumination, and the max frame rate is ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello user,
Thank you for your interest in our DLP Technology. The DLP4710 DMD only supports bottom illumination. The supported frame rates for a 1920x1080 resolution is 5 - 62 Hz.
A frame rate up to 120Hz can be achieved by reducing the resolution.
Best regards,
Nadine
Does DLP3010 support a frame rate of 120HZ with resolution 1280x720, or it also need to reduce resolution to rate up to 120HZ?
Hello User,
The DLP3010 chipset supports a frame rate of 120 Hz with a resolution of 1280x720. In general the resolution and frame rate limits in combination with each other are depending on the Pixel clock of 150 MHz which is the same for both 4710 and 3010 Chipsets.
Best regards,
Nadine
Is there any possible solution to make DLP4010 support a frame rate up to 90-120Hz without reducing the resolution?
Thanks!
Best Regards!
Hello User,
Thank you for your interest in our DLP Technology.
The PCB schematic can be found on the DLP LightCrafter 4710 Tool folder or under following link:
Best regards,
Nadine
Dear Nadine
Is there another DLP chip set available to ashive 480 HZ?
THANKS
MOKHTAR