We are working with the DLP NIRScan Nano and would like to learn how to control the mirrors. Do you have some documentation and examples concerning how we can learn to control the mirrors for non-standard configurations.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We are working with the DLP NIRScan Nano and would like to learn how to control the mirrors. Do you have some documentation and examples concerning how we can learn to control the mirrors for non-standard configurations.
Hi Dana,
The mirrors in the NIRscan Nano are controlled by patterns generated in the Tiva firmware which are then sent to the DLPC150 controller. These patterns are generated by the DLP Spectrum Library. This library includes pattern generation and spectrum interpretation functions for two types of scans: Column and Hadamard scans with programmable start and end wavelengths and programmable pattern widths, which affects system resolution. All of these software packages are available on the DLP NIRscan Nano EVM page.
If you would like to experiment with other custom types of patterns, there are two potential methods:
During evaluation and initial development, the first option will certainly be a faster way to experiment.