This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

A flash of red LED when LCR4500 is powered on

I got a few LCR4500s.One of them has a issue red LED flashes when the LCR4500 is powered on. After that, it works fine. Others don't flash(It's fine). I think it has something of problem around power circuit. I would like to know the cause.

Please provide something of information.

Regards,
Uryyy

  • Hi Uryyy,

    Are you referring to the red LED in the light engine or a red status LED on the LightCrafter. If it is a status LED, could you provide the reference designator for the LED? Could you also let us know any modifications that have been done to the EVMs, the SW/FW versions you are using and how you are testing the devices?

    Thanks,
    Clinton
  • Hello Clinton,
    
    The issue can be seen with my own eyes. I updated the latest firmware(DLPR350PROM-3.0.0) on Lightcrafter4500, but the issue hasn't been solved. 
    Before that, I had used the factory settings' LCR4500.(Forgot the version.)
    
    Thanks,
    Uryyy