This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Looking to control a DLP 4000 through Matlab or other software

Hi,

I'm currently using a DLP4000 Starter kit.

I'd like to avoid going through the DLP Discovery 4000 Explorer software as it only runs on Windows XP and doesn't allow me to do an automated update of the DMD.

I'd like to be able to control the DMD through Matlab (loading a picture and reseting the DMD).

I've checked the datasheet I've got and I don't have these three that would be very useful to me:

-Discovery 4000 API Programmer's guide

-Discovery 4000 API Source code

-Discovery 4000 API Programming Sample Codes

Could you send me these files or do I need to see directly with the company that sold us the DMD?

Moreover, as far as I understood from different posts on the forum, I'll need the *.ocx, *.dll and *.h files to control it without using the TI software.

I have the .dll and .ocx files (I have D4000_usb.dll and DDC4000.ocx) but I don't have any *.h file. Can you supply me this file and confirm me that these are the only files I'll need to control the DMD? If not can you let me know who could provide the *.h file.

Regards,

Antonin