This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC350 Validate Data Command Response

Genius 5960 points

Other Parts Discussed in Thread: DLPC350

Hi,

Please tell us about DLPC350 Validate Data Command Response.

Validate Data Command Response Register
- Status of post sector settings(bit3)

Please tell me the meaning of this bit.

What is the condition that a flag is set?

Best Regards,

hamada

  • Hi Hamada-san,

    I shifted your question into the forum which covers DLPC350 topics. Someone from our team should have an answer for you here soon.

    Thanks,
    Trevor
  • Hi, Trevor.

    Thank you for reply.

    Did you move anywhere in the forum?

    Since DLPC350 a question,
    Although we believe that good at this forum.

    Best Regards,
    hamada
  • Hi Hamada,

    Flag is set under following conditions:

    For Pattern Definition there are two settings with respect to display.

    1. Patten Exposure (in us) -> The time for which pattern is exposed

    2. Pattern Period (in us) -> Total time allocated for the pattern

    Following options possible

    Option-1: Pattern Exposure = Pattern Period

    Option-2: Pattern Period > Pattern Exposure where, Pattern Period - Pattern Exposure must > 230us.

    For Option-2, let's say, Pattern Exposure = 5000us and Pattern Period = 10000us, now basically after exposing the pattern for 5000us the content must be cleared on the DMD, this is possible iff we are selecting, a flag, refer DLPC350 Programmer's Guide (Table 2-68. Pattern Display LUT Data - Pattern Definition Command
    ), BYTE2, BIT1 = 1, Insert black-fill pattern after current pattern.

    If you are not setting this flag, then the BIT3 error flag in Validate Data Command Response Register (0x7D) will be set.

    Regards,
    Sanjeev 

  • Hi, Sanjeev.

    Thank you for reply.

    OK. I understand the conditions.

    Let me check it additionally, please.
    What does this flag mean?

    Best Regards,
    hamada
  • Hi Hamada-san,

    It is a warning flag that the last bit of the Pattern remain after the exposure completion. By appropriate definition in the pattern LUT, the controller will run a 230us black vector that will clear out the content on the DMD after exposure completion.

    Regards,

    Sanjeev