Hi,
I am using python to control the DLP3000. I am using Software command (Next) to go from one pattern to another in the sequence. Using checkerboard 1-bi depth patterns all works great. However, when trying to project a sequence of 8-bit sinusoidal pattern I see that the DLP projects only binary images (like stripes).
What can be the cause?
My configuration setting is:
settings = {
"depth": 8, # Bit depth
"num": 3, # Number images
"include_inverted": 0, # Inverted included yes or no
"trigger": 0, # [0, 1] [SW command, Auto trigger]
"delay": 0, # Initial delay microseconds
"period": 20000, # Full microseconds
"exposure": 10000, # Exposure microseconds
"led": 0 # [012] [RGB]
}
I have tried several period and exposure timings and nothing seems to work although I should remember that I am controlling the sequence move by software command.
Thanks a lot for your time, Pepe