This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Keystone of the LightCrafter 4500 using DLPC350

Other Parts Discussed in Thread: DLPC350

According to the DLPC350 manual, there is an adjustable 12 degrees for the tilt angle of the projector. I was wondering how to adjust this? Is this adjustable using the GUI or does it need to be encoded to the chip? If it is adjustable using the GUI, where is the manipulation in the GUI?

  • 12 degree refer to the individual mirror tilt. The mirror tilt based on the data bit is loaded under each mirror. The controller takes care of formatting the incoming data prestored or streaming video and convert them into bits.
    There is no option to change the tilt degrees, it is fixed. +12 (for value '1') or -12 (bit value of '0')
    Regards,
    Sanjeev