This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can TFP401A(U6:DVI I/F) be eliminated from DLP Lightcrafter PWB design?

Other Parts Discussed in Thread: TFP401A

Hello,
I have a question about DLP Lightcrafter from my customer.
They plan to build their PWB similar to DLP Lightcrafter.
Thay are going to eliminate TFP401A(U6:DVI I/F) on their design
because they do not need external video display. They are concerned
about DM365 operation when eliminating TFP401A. The DM365 can
communicate with TFP401A via I2C.

Their questions are as follows when eliminating TFP401A.
1.Does DM365 firmware run normally without getting stuck
when initializing TFP401A?

2.Does DM365 firmware run normally without getting stuck
when selecting external HDMI source?

Please provide suggestions for avobe questions.

Thank you.
Best regards,
S.Watanabe