Hi,
I'm evaluating a DLP4500 for a 3d Printer.
I need the DLP to boot in MANUAL LED SELECTION and set max current to 30 so I've edited these values using the 3.0.0 GUI and created a new default.ini with the new values. When I apply this ini file (solution) it works OK. I've also made a new firmware image (based on 3.0.0) with this modified .ini settings.
The problem I see is that when the DLP boots all values are correctly set according to the new .ini (LED currents i.e) except that the LED SELECTION is in AUTOMATIC and I need and saved MANUAL Mode (I need BLUE Led always on, no LED multiplexing).
The new .ini contains a line to indicate manual mode:
DEFAULT.LED_ENABLE_MAN_MODE 0x1 ;
But it seems that DLP firmware doesnt recognize it.
( when I Apply this new .ini in the 3.0.0 GUI it correctly sets the MANUAL LED SELECTION Mode, so I'm sure that the .ini is OK)
Thanks in advance.
Regards,
Guillermo Molina
Buenos Aires
Argentina