This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Window Coating

Other Parts Discussed in Thread: DLP2010NIR, DLP4500NIR

Are any of these devices available to order without a coating on the window?

DLP7000 (400-700 nm)

DLP9500 (400-700 nm)

DLP7000UV   (363-420 nm)

DLP9500UV   (363-420 nm)

  • Hello Robert. 

    We do not offer any DMD's that do not have an optical coating on the window.  They have either a Visible or UV coatings for the DMD's listed above.  We also have two NIR coated chips, the DLP2010NIR and the DLP4500NIR (in two package styles).

    These coatings are on both sides of the window.

    I wish we had different news for you.