Hi
I want to use other cpu (a fpga) to comunicate with the dlpc150. but the dlpc150 is configured from a external SPI FLASH. how can I upload the firmware of the dlpc150 when i don't use the platform of Tiva? When i use dlp4500nir and dlpc350,there is a method to configure the flash ,is there a similar way to configure the flash for dlpc150?