This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB driver issues and unable able to flash firmware



I was getting an error while trying upload default firmware to the my DLP Lightcrafter 4500. The error I was getting was: Unable to read flash manufacturer ID.

In order to troubleshoot the issue, I came across one solution where the user suggested to uninstall and reinstall USB drivers. Unfortunate I did something wrong in the Device Manager of my Windows 10 PC.  After uninstalling and reinstalling the USB drivers, DLP is not being detected by the the GUI program. When I launch the GUI program, it says my DLP Is not connected. I am pretty sure the USB drivers are installed. 

Please help.


See attached picture:

  • Use another computer to connect to the hardware. If it is able to detect and connect then still there is a problem on your Windows 10 machine else you might have corrupted the flash and you are not able to boot the board. Just in case try using another USB cable.
    Regards,
    Sanjeev
  • I have been using another PC to upload the firmware. Until now my second PC was able to properly upload the firmware, but now once again I started running into the "Unable to read flash manufacturer" issue. I think there is something wrong with the GUI software. I also tried redownloading the GUI software, but the link on TI's website does NOT work. www.ti.com/.../dlplcr4500evm