Hi
I use a DLPC3438, DLPA3000, DLA3010.
Voltage level and sequence of VRST, VOFS and VBIAS is normal, as shown below.
VRST = -14.25V
VOFS = 9.82V
VBIAS = 17.58V
I expect that the state of DLPA3000 is ACTIVE1.
I would like to know whether the VLED is on in order to do to be ACTIVE2.
SPI of DLPA3000 is connected DLPC3438 SPI1. so I can not control (Read/Write) ILLUM_EN (0x01).