Hi,
I am able to "PLAY" six 8-bit frames from two different Image Indexes with frame period set to 15000us and exposure time set to 10000us.
But I have trouble playing twelve 8-bit frames from four different Image Indexes with the same frame and exposure timing. The images seem to overlap and display corrupted images after a while.
If I understand the user manual correctly, I have to keep 200ms between each 3-frames to allow the next image to load from flash using the "VARIABLE EXPOSURE" control. But it does not function on Firmware 2.0. I have the need to use the Firmware 2.0 as Firmware 3.0 has issues with using "PLAY ONCE" mode.
It seems that when the Firmware was upgraded from 2.0 to 3.0, it caused the appearance of some bugs with this regard.
Has anyone found a workaround to "PLAY ONCE" for twelve 8-bit frames from 4 different image indexes?
Thanks in advance,
-John