This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I Just Need a Low-Resoltion Projector ....

Other Parts Discussed in Thread: DLP2010

Kind sir/madam:

I only need to poroject a low-resolution image onto an area about 1sq ft. The distance from the projector to the target surface is about 1 foot.

The image would consist of large letters, and/or icons.

For example: I could project a round image of a speedometer, and the words "Slow Down". I don't need high resolution. Just a projection technology and a pathway to get there. Another projection could be a similar icon and letters.

Might the people at TI have something for that?

 

Thanks,

Michael A. Banak