Hi,
I have two beginner questions with regards to the DLP NIRscan Nano DLPNIRNANOEVM.
First question is with regards to the Bluetooth/Scan switch. Is it possible to have it turned on by default when opening the device? I am looking to incorporate the DLP NIRscan Nano in a larger experimental setup and having to manually click on the little Bluetooth/Scan switch everytime I want to use the device is quite annoying.
Second question is with regards to the battery. I will order the recommended battery pack for this unit:
Tenergy Li-Polymer 3.7V 1700mAh (103450) Battery
Will the battery charge automatically if I connect the device to a wall plug or a computer using a micro USB cable?
Thanks!