Hi there !
I would like to know the pattern sequence when DLP4500 is set to display multi-bits in pattern sequence mode. For example, if the bit depth is set to be 8, from R0 to R7, does it display the 8 bits in turn from R0 to R7? Because when R0~R7 was 127(01111111 in binary) in decimal, I got the following waveform. The rectangle shows a period. It seem that DLP4500 first displayed R0~R5, after some time, it displayed R6 (or in reverse). And it seems that the bits are displayed in different orders under different settings.