This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Single line DLP

hi ,

i wanted to know if there is such a thing as single line DLP.

i want to scan with the singe line(one dimension) to project an image (two dimension) by  using a mirror.

thank you ,

yuval

  • Hello Yuval,

    Welcome to the DLP Advanced Light Control section of the TI-E2E community.

    We do not make a single line DMD, although there is nothing that prevents you from loading everything except one line as all off and then load the line with required data.

    I hope this is helpful,

    Fizix

  • Hi Yuval,

    in addition to the answer of Fizix above I give you the hint that there is a special DMD function available for ViALUX ALP-4 Controller Suite which is called AOI (=area of interest). That function use part of the DMD (defined number of DMD lines). With the help of this function the switching rate of the micro mirrorrs can be increased up to the DMD chip limit of 50khz (if you use just 1 or 2 lines).

    For further details about that function please contact me with dlp@vialux.de

    Philipp

    (ViALUX GmbH, TI Design House Partner, Germany)