Hi I have a project for near eye HMD that will use dlp with LED as light source and I was considering evaluating the DLP4710 for our project however we have a non standard refresh rate requirement we need a minimum of 240hz rgb refresh rate but would prefer 480hz and yes there must be a good reason we want to do that :) I couldn't find yet details about max possible refresh rate with DLP4710 and if it cant handle that rate any other model that would be capable of handling it but must be full hd resolution and should be at affordable price range no more than $200 in 1k quantity...