Hello everyone,
I'm currently having problems try to make use of the " Multiple bit and multiple color sequence" setting of the DLP LightCrafter Control Software 5.0.0 for Windows. When I enable this option, it asks me to upload three different files. The first two are described on the user's guide. There are also example provided of these 2 types of documents. However, the third file " Image List File", is missing from the examples. It is also unclear what type of file or what the content of this file should be. If anyone could offer an example or a more detailed explanation on how to use this setting that would be extremely useful. I work with a DLP LightCrafter (DLP 0.3 WVGA chipset).
Thank you,
Regina