Hi
Since I have to write a simple c++ program for controlling DLP 6500, I have followed the steps in the guide http://www.ti.com/lit/ug/dlpu042/dlpu042.pdf and installed the ALC SDK.
In QT Creator I'm able compile image_file_io.cpp with no errors, so I'm guessing the SDK is correctly installed.
However I have not much experience in programming c++ and do not understand the Doxygen-documentation in detail, so I was wandering if anyone out there could provide me with an example of how to connect to DLP 6500, put it in the 'Pattern on-the-fly mode' and upload an image?
It would be much appreciated. Also I would be grateful for any hits that could point me in the right direction.
Thanks in advance
Nicolai