Hello!
My name is Henry, and I use a DLP9000 in conjunction with my current research. Briefly, I am using an HDMI connection to make the DLP9000 a 'second display,' and display my desired image sets on it through this HDMI connection. I then shine light (405 nm) onto it, and use a USB camera (an Amscope MU035) to view the resultant image.
My images show up successfully, but the video data shows that the projected image is 'flickering.' Closer inspection at lower exposure times reveals 'scanlines' moving across the surface. Previously, when uploading the images to the DLP's internal memory, there were no flickering or scanlines. Is there a way to eliminate these scanlines? Is this an issue with the DLP9000?
Thanks for your time!
Henry