Hello
I am working with a DLP Lightcrafter 9000 EVM. Following the instructions to turn it on for the first time include:
- Plug in the power supply
- wait 5 seconds for it to boot up
- Connect USB cable from device to computer
- Operate through the downloadable GUI
When I plug in the power supply, 2 LEDs come on - D11 and D12 - indicating it is receiving the 12V of power. However, the remaining LEDs do not come on, nor does the mirror display become active and begin its continuous pattern sequence.
Is there a chance the software pre-loaded on the device was not pre-loaded or somehow was erased? How can I fix this issue?
Thanks