This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question about the camera uesd in the TIDA-00254 design(using the DLP lightcrafter 4500)

If i want to use the camera of other brands instead of  using the Point Grey camera, what requirements should the cameras meet? (including resolutions and the  frame rate,etc.) And is it difficult to modify the source codes for using the other cameras?

  • The camera requirements are going to be somewhat dependent on your application. In general, we recommend that the camera's resolution be at least 4 times the resolution of the projector. The frame rate of the camera will depend on what speed you need to run your application. It should not be terribly difficult to modify our source code to include a new camera module - take a look at how we've instantiated the PointGrey camera for an example.

    Hope this helps,
    Paul