Hi,
Just a quick question regarding how the Lightcrafter 6500 GUI works with the input trigger. For my application I am using an external trigger to cycle through prestored patterns in the DMD as part of a sequence, in a highly synchronised way.
The trigger works, and when input 1 goes high, the patterns change. However, I have been wondering if it is possible to set the GUI such the the exposure of each pattern is automatically adjusted to the trigger signal and not controlled directly from the GUI? Currently, it receives an impulse, then projects a pattern for the time specified in the GUI and then goes blank until another impulse is received. Instead, we need it such that when an impulse is received a new pattern is projected, and stays projected until another impulse arrives, which advances to the next pattern and so on.
So far we have been getting around the issue by manually adjusting the exposure to match the frequency of the input trigger, but this is not optimal and takes a lot of time. Is there a quicker and better way around the issue, by somehow getting around the exposure control in the GUI?
Many thanks
Alex