Dear all,
Whether the smooth picture technology is used in 0.45 dmd diamond arrays(912*1140) displaying?
wanna know how its pixels correspond to 1280*800 picture. Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Paul,
Thanks again.
As you said,project image in pattern mode.
If project image with circles,I need create an 16:10 picture(1280*800) and get it to 912*1140 in image editor .Then input the lightcrafter and project.That is recoved to circles.
If line images will be projected,I just need to creat 912*1140 images and inout the light crafter to projected.
That is right?
Joyce
paul,
I have read question 3 in the FAQ and some questions are still puzzled me:
*I know that incident illumination orientation is vertical to the hinge axis. I wonder that the incident illumination has any influence on image display?
* What does 'grayscale patterns' refer to?I don't understand why it is used,the “jagged” edges can produce the appearance of an intermediary pixel or “sub-pixel” when viewed or captured through a camera that has greater resolution than the projected pattern. The appearance of these sub-pixels can provide additional resolution in some applications?
Hope to reply,
Joyce
Joyce,
The jagged edges comment is primarily a human perception issue. Basically with small pixel sizes and a diamond configuration, the human eye will perceive more detail on the jagged edge than is actually there. This really isn't important for non-display applications and with the Lightcrafter the effect will probably be minimal.
The primary advantage of the diamond array is that the orientation of the light source allows for a more compact optical design.
Thanks,
Paul
Paul,
Sorry to disturb you.
I know something that 912*2:1140=1280:800=16:10 and see some word " two frames" somewhere . So I want to know why 912*1140 arrays can display a 16:10 image. what is the hypostasis about the diamond array in lightcrafter 4500.
And with your recommendation, I carried out some experiment and the result of calibration and 3d measurement experiments were not good.
I don't know why? ps. The measurement accuracy of the 3d measurement system that I hope is 50um. I don't know whether some wrong with my operation or this product is not propitious to my experiment and objective.
Thanks
Joyce
Joyce,
The system that is mentioned in the paper you provided sounds like our UHD system. The system uses the speed of the DMD and special optics to use single mirror and make it project multiple pixels. Here is another article that might help you understand.
This ability is NOT something that the DMDs do natively. It relies on having a complete system design around it to make this possible. We are simply utilizing the fast switching speed of the DMD to make this possible.
Thanks,
Paul