I understand the FPGA starts configuration with "nCONFIG" pin going to high after power on.
And nCONFIG is connected to GIO46 of DM365. This line should be controlled by DM365 s/w
properly. But GIO46 keeps as GIO input mode. The line is observed about 2.2V because external
pull-up resister is connected.
I guess the FPGA starts configuration when nCONFIG goes to 2.2V from 0V at power on.
In this case state of GIO23 impacts the high level of DO output(FPGA Flash) in the beginning
of configuration. But the FPGA retries configuration with "Auto-restart configuration on error"
option. Then configuration will be succeeded when GIO23 is stabled.
Please check DM365 s/w and control GIO46 properly. Also please check operation of GIO45(nCE).
Thank you.
Best regards,
S.Watanabe