Hey guys,
I'm a little stuck here. I want the LightCrafter 6500 to boot with HDMI receiver activated so I don't have to switch the mode manually. As far as I understood I need to reflash the firmware with the HDMI/DP receiver flags activated.
The problem is the following: I can't find the firmware nor can I find any information about it. The documentation only say "locate the firmware" but the 'DLPC900REF-SW-2.1.1' package doesn't contain any firmware *.img files. I even compiled the UI from the containing source code but still I can't locate anything remotely looking like a firmware package.
Can someone please give me a hint where to look for it or send a link to a proper documentation on how to get it?
Thanks very much,
Stanislav