Hi All,
I need to display bichromatic and monochromatic images on the DLP4710 kit.
For this purpose , I would need to modify the duty-cycle values of the Look Structure in the DLPC3439 controller.
The command 26h allows to read those values (byte 1-6) and the command 22h allows selection of the Look table.
My need consist in modifying the Look values which are in Flash (likelly in 41h-4Fh, addresses marked as RESERVED in the User's Guide).
Can you please let me know if this is the right procedure ?
The desired result is to change the duty-cycle to 50% for Green and 50% for Red for the bichromatic setup and 100% for the Green in case of monochromatic setup.
Thanks for your help.