Hi,
We are starting a project to design our light scanning system. Its will be based on DLP® 0.45 WXGA NIR DMD and DLP® Digital Controller for the DLP4500 DMD. We are finding very little that explains the process in designing the entire system. There was a good bit that discussed the optics but not what other electronics are needed and what software programming is needed to tie it all together.
We want to synchronize a self-made laser source(850 nm) with the DLP system by LabVIEW. Which product should we purchase? The LIGHT CRAFTER 4500? But this is to expensive for our end product. We must design the entire system and eliminate what is not necessary.
Thank you.