Hi Everyone,
I am an undergraduate student at the University of Nevada, Las Vegas and am in need of assistance for a project I am working on. Essentially, I need an optical engine that can have a display area of approximately 3" x 4" at a maximum distance around 5 inches and projected at around 45 degrees. So instead of having a large image, which projectors are used for, I need the opposite. I've done research on the EVM's Ti has to offer, but none of the spec sheets detail the minimum focus distance and I don't think any of them can achieve what I need based off the throw ratios. I am new to this technology and how to properly describe what I need in proper terminology, so I apologize in advance. Any help and guidance would be deeply appreciated.