Dear,
My research group is building an interference exposure system using 266 nm laser, and we are looking for the DMD arrays as the mirror adjusting angular.
However, the lowest specified wavelength for the DLPs on the TI website seems to be 363nm.
We have some questions.
1) Which DLP do you recommend? DLP7000UV or DLP 9500UV?
2) Can DMD be used in 0, 5, or 10 degree state?
3) Can DMD be used under 266 nm laser and then what is the percentage of the reflection?
I am looking forward to hearing.
Best Regards,
Kazuki