Hi fellows,
I recently read about using pattern sequence mode for finer details in 3D printing application
"in order to bypass that processing and directly control individual micromirrors, the projector must instead be used in "pattern mode". In pattern mode, the intensity of each projected pixel depends only on the gray value of the corresponding individual pixel in the source image, regardless of the location of that pixel. Because of that, parts printed in pattern mode can reproduce finer details than parts printed in video mode" ( http://www.instructables.com/id/Ember-Printer-Using-Pattern-Mode-for-Finer-Details/?ALLSTEPS)
I would like to know if its possible to send the slice images from a beaglebone which also would read the trigger from software?
Have anyone try to interface beaglebone with lc4500?
thanks.