This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP Lightcrafter 9000 cannot be detectedd



I newly bought a DLP Lightcrafter 9000 with EVM. Today I tried it out but found out that after I connected it with a 12 V power which is the recommended one, only D11 and D12 LED lit on, D5 did not light on, D7 and D9 did not toggle. I also connected the EVM with my PC and opened the latest GUI 3.0, but it indicated that my EVM is disconnected. Is my DMD damaged? What can I do to save it? Thanks!