Hi,
in the manual of the LightCrafter 4500 it says "Exceeding more than 4.3 A for continuous or simultaneous LED operation can damage the LightCrafter 4500 LEDs.". The default LED values applied to the formulas provided to calculate the LED currents result in a total current usage of 7.3A (unless I am calculating it wrong). Does that mean that with the default LED currents it is unsafe to display an all white image for an extended amount of time? Is there a different between video and pattern mode? In pattern mode the projected image seems to be brighter. My main concern is: is it safe to display an all white pattern in pattern mode for a long time? If not, what is the recommended maximum time?
Many thanks,
Jan