This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question regarding trigger configuration



I am wondering if it is possible for the DLP light commander to both take an external trigger but also generate a trigger output?

Thanks in advance for the help.

Regards, Bing

  • Hello Bing,

    It was designed for both functions, but for clarification are you asking if it can do both at the same time?  If so the answer is yes.  

    Please refer to the following software user manual from Logic PD:

    DLP® LightCommander™ Control Software User Manual <-- click on the link to view.

    Please refer to section 7.4 (page 36) for information on input trigger [called Sync].

    Please refer to section 7.10 for information on output trigger(s) [called "Output Syncs"]

    I hope this helps.  Let me know if you have further questions.

    Fizix