This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI GUI and actual settings f/w 3.0.0



When I set Pattern Display Data Input Source (USB: CMD2: 0x1A, CMD3: 0x22) to 0 (Pattern Display Data is streamed through the 24-bit RGB/FPD-link interface) and Pattern Trigger Mode Selection (USB: CMD2: 0x1A, CMD3: 0x23) to 0 (VSYNC serves to trigger the pattern display sequence) via USB and then recheck them but read command everything is right, but than when I run TI GUI v.3.01 it shows me that Patter Source is Flash instead of VPort and Trigger mode is External instead of VSYNC, why?

Thanks.

  • Hi Nik,

    I believe this is due to how that particular portion of the GUI works. Those settings are not reflecting what is already set on the Lightcrafter, those are settings that will be applied to the sequence that you build using the GUI, if that makes sense.

    If you hit the "read" button, you should be able to retrieve the sequence settings.

    -Paul