Hello this is Gilwan.
I have a questions as below.
- Can we use DLP4710 for 3D printer application?
- If we apply UV 405nm, How about window transmittance and reflectivity of DMD micro mirror?
- If we apply 405nm UV, what is the expected DLP4710 device life time?
- I do not clearly understand the meaning of ILLuv (Illumination wavelength <400nm) which is in the recommended operating condition of DLP4710 manual. Would you please let me know the meaning of ILLuv?
- Is there any limitation of the maximum power of UV LED which can be applied to DMD? If yes, what is the main reason?
- New 4710 EVM Gen2 focus range looks 40 ~120inch compare to old 4710 EVM focus range 5~120 inch. Is there any way we can apply 5 inch focus with 4710 EVM GEN2?
My personal e-mail is gilwancho@gmail.com