I see that the DLP4500 is aimed for advanced light control and the DLP4501 is for video. However the optical engine that is quite reasonable for our purpose has the 4501 on it, although we need to send in bit frames as fast as possible. I cannot seem to ascertain the wiring diagrams for both chips to compare to see if the 4501 is throttled down relative to the 4500. If one could ( magically) design and build our own interface, would the 4501 have the same capabilities as does the 4500? We have a lot of design capability here and are thinking along these lines, but would like to start with one of the available and low-cost light engines that you recommend from China.