Hello
I want to know why the lenses aren't simply Plano convex lenses? I see from the assembly drawings that the lenses, got from Optimax, have a little curvature in the "plano" region. Why this? Is it a reason linked to focusing problem?
Moreover I'd want to know if I may change all 6 lenses and replace them with other 6 (plano convex) which work in spectral range (900nm-2500nm) of my interest.
(I am worried that if I put 6 plano convex lenses in the system I would ruin the focusing or something similar)
Final query: Optimax doesn't seem an online "Store". Do you think that if I request them 6 lenses with same dimensions of those placed in NIR scan nano EVM, but working in the spectral range mentioned above, they might provide them to me?
Thank's a lot