This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Connecting several LightCrafter 6500 EVMs to one PC

Hello,

I also have trouble to control two Lightcrafters with a PC via USB.
Should your answer be worked for Lightcrafter6500 as well??

I am using two Lightcrafter6500, then I cannot find how to change the IP address using the GUI for Lightcrafter 6500/9000.
Either Lightcrafter6500 can be connected to the GUI, but not simultaneously.
And I downloaded the LightcrafterGUI, which might be mentioned in your first link, I cannot connect either Lightcrafters to the GUI.
  • Hello and welcome to the DLP Forums. Thank you for your question!

    The advice given in the Lightcrafter forum does not apply to the Lightcrafter 6500, they are quite different devices. The Lightcrafter 6500 (LCr6500) does not have an IP to be changed, it uses USB 1.1 to communicate to the computer.

    Unfortunately, it is not possible to connect more than one LCr6500 to a computer at a time and have the GUI control them.

    -Paul
  • Dear Paul,
    Thank very much for the quick and clear answer! Then I will just use two computers to control them.

    Yours,
    Kozue